This directory contains all the script file made to run different simulators.
The following sections gives brief descriptions about the scripts
1. run_all_scr--This is an interactive script for running simualtion.

Flow of questions:

First Questions asked by script to user is :
Q1:
Welcome Independent Clock Quad Hotlink-II Behavioral Model(Verilog/VHDL) Simulation Env
                    1. Verilog Model(Default)  
                    2. VHDL Model
A1: 
The user can type 1 or press enter for simulation of the Verilog Model.
The has to type 2 for simulation of the VHDL model.
######################################################################################
If the A1 is  1  or user press enter 
######################################################################################
the next question asked by script to user is 

Q2 : 

Choose a simulator : 
 1. Verilog-XL (Default) 
 2. NC-Verilog 
 3. ModelSim

A2: If user wants to run the simulation using Verilog-XL, the user has to type 1 or press enter
    If user wants to run the simulation using NC-Verilog, the user has to type 2
    If user wants to run the simulation using ModelSim, the user has to type 3 

Next quaetion by script to user is 

Q3: 

 Which testbench you want to run: 
 1. TX-BIST 
 2. TX-ENCODER ENABLED 
 3. TX-ENCODER DISABLED 
 4. RX-BIST 
 5. RX-MODE 
 6. TX-RX LOOP BACK MODE 
 7. RUN all modes in the above sequence

A3: Type 1 to run TX-BIST 
    Type 2 to run TX-ENCODER ENABLED
    Type 3 to run TX-ENCODER DISABLED
    Type 4 to run RX-BIST
    Type 5 to run RX-MODE
    Type 6 to run TX-RX LOOP BACK MODE
    Type 7 to run all modes in the above sequence
Next question asked by script to user is
Q4: 
 Do you want to remove log and VCD files(Y/N) from rpt directory : Default is No
A4: If you want to clean the rpt directory  type y other wise press enter 

Next question asked by script to user is
Q5: Do you want to dump VCD file(Y/N): Default is No

A5: If you want to dump VCD file(s) type y or Y  else press enter 

Q6: Do you want to on the DEBUG MODE(Y/N) : Default is No

A6: IF you want to run the model in debug mode type y or Y  else press enter 

If the answer of the Q6 is Y or y then the following question will come:

Q7:
Do you want to on TIMING MONITOR(Y/N) : Default is No

A7: If you want to on TIMING MONITOR type y or Y else press enter 

Q8: Do you want to on UNKNOWN HANDLER(Y/N) : Default is No
A8: If you want to on UNKNOWN HANDLER type y or Y else press enter

Q9: Do you want to on Operation Related Message(Y/N) : Default is No
A9: If you want to on Operation Related Message type y or Y else press enter 


######################################################################################
If the A1 is  2
######################################################################################

q2:
 Choose a simulator : 
 1. NC-VHDL(Default)      
 2. ModelSim

a2: type 1 or press enter to run simulation using NC-VHDL simulator
    type 2 o run simulation using ModelSim simulator

q3 : 

Which testbench you want to run: 
 1. TX-BIST 
 2. TX-ENCODER ENABLED 
 3. TX-ENCODER DISABLED 
 4. RX-BIST 
 5. RX-MODE 
 6. TX-RX LOOP BACK MODE 
 7. RUN all modes in the above sequence

a3: 

 Type 1 to run TX-BIST
    Type 2 to run TX-ENCODER ENABLED
    Type 3 to run TX-ENCODER DISABLED
    Type 4 to run RX-BIST
    Type 5 to run RX-MODE
    Type 6 to run TX-RX LOOP BACK MODE
    Type 7 to run all modes in the above sequence
Next question asked by script to user is

q4 : 
    Do you want to remove all log and VCD files from rpt directory(Y/N): Default is No 
a4: If you want to clean the rpt directory  type y other wise press enter

Next question asked by script to user is
q5: Do you want to dump VCD file(Y/N): Default is No

a5: If you want to dump VCD file(s) type y or Y  else press enter